Intelligent, reliable and efficient district heating systems
District heating systems distribute mass amounts of heat over potentially large areas. And in order to keep the customers happy, three factors are important: reliability, efficiency and intelligence. Grundfos supplies a wide portfolio of pumps to power plants, in boiler houses and in the distribution lines, all combined to ensure that heat is distributed optimally – satisfying all heating demands throughout the district heating network.
Keeping a district heating system running reliably requires attention to detail. Grundfos can help with that. Pressure, flow and temperature are the three main parameters to consider, but water purity and pH-value also play a part in deciding the level of wear and tear in your pipes. However, these parameters can be controlled with a flow filter system and an effective water treatment system, both of which feature Grundfos pumps.
Grundfos iSOLUTIONS in district heating
District heating has the potential to reduce CO2 emissions and heat losses while increasing consumer comfort. Discover how Grundfos iSOLUTIONS can help your district heating systems run with lower temperatures and optimal efficiency with the use of intelligent solutions.
Reduce heat losses and save costs with Grundfos iGRID temperature zones
Use Grundfos iGRID temperature zones to add digital demand-driven heating zones to your district heating network and reduce heat losses, deliver low-cost heating and open up for heat generation from renewable energy sources.
Download whitepaper and learn more.
District energy application guide
Learn about the growing need for district energy to combat the world's energy problems – today and tomorrow. Explore the different installations, networks and benefits of district heating and cooling. And why district energy is the answer to smarter cities of the future.
Interested in improving your knowledge of this application?
Find out about the latest studies of pumps and systems, where to use Grundfos solutions and how to achieve the best performance, or search Grundfos research & insights for specific learning materials, articles, white papers, videos and much more that benefit your solution.
Get answers to your questions about this application
We have gathered frequently asked questions and their answers in one place. See the most frequently asked questions below or go to the Grundfos FAQ for a complete list of answers to your questions about our products.
How does one read a pump curve of a heating pump?
The pump curve of a heating pump displays the feed rate on the x-axis and the delivery head on the y-axis. The pump curve shown in the graph is curved, dropping off from left to right.
Every possible duty point of the pump is shown on the pump curve where the dependencies are as follows: high feed rate = low delivery head; low feed rate = high delivery head.
In a heating system, a system curve emerges as a function of the system hydraulics. This curve intersects with the pump...
What is the heating system filling water requirement?
VDI Guideline 2035 Part 1 has been in effect since 2005, and VDI Guideline 2035 Part 2 has been in effect since 2009. These guidelines represent recognised rules of the technology. Ongoing technical advances as well as efficiency improvements and energy optimisation mean that modern heat generators and heating pumps are designed with lower tolerances than they were in the past. These technical advances have led to increased demands placed on the medium pumped in the system, as defined by ...
Why does the heating system not reach a sufficient temperature?
Possible cause of the fault
Automatic night set-back is active
The hydraulic conditions have changed. The pump must adapt to these.
When night set-back is activated
Switch on night set-back using Button 4 (for MAGNA, use Button 3).
In "AutoAdapt" mode
Possible cause of fault: The "AutoAdapt" function is unable to correctly adapt the heating system.
Remedy
Why is the heating system making noise?
Possible cause of the fault
The flow rate is too high
This can be resolved by setting the pump to a setting other than "AutoAdapt"
Note the pump setting that appears on the display.
Then use Button 5 to switch the pump to "AutoAdapt". (for MAGNA, use Button 3)
If the supply of heat is sufficient at this point, leave it at this setting.
If the supply of heat is not sufficient, restore the previous setting...
Circulator pumps
Hydro boosters
Endsuction long coupled single stage
Endsuction close coupled single stage
Endsuction close coupled multistage
Horizontal split case pumps
Inline single stage pumps
Inline multi stage pumps
Booster set
Enhance your knowledge
Find out how to get reduced energy consumption, increased comfort and unsurpassed operational reliability for your application. Read our customers' stories about how they benefit from the Grundfos approach to intelligence, water and energy, or search Grundfos research & insights for more learning materials, articles, white papers, videos and much more that benefit your solution.